Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Can a Single-Pole MCCB be Installed in a Circuit Breaker Enclosure?
Issue: Determining if a single pole MCCB is possible to install on a circuit breaker enclosure

Product Line: Enclosed Circuit Breakers and PowerPacT MCCB's

Resolution:

No, it is not possible. The circuit breaker enclosures only allow 2 or 3-pole MCCB. However, it is possible to install a two-pole breaker and use only one of the poles for that application.

Schneider Electric Canada
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
  • Register Your Product
  • Blog
  • Legal Information
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings