Issue:
Summary of when I-Line Interiors were introduced and obsoleted
Product Line:
Panelboards
Environment:
I-Line Panelboards
Resolution:
NOTE: The year introduced column is when they were first offered and the obsoleted column is when they were completely obsoleted.
Summary of when I-Line Interiors were introduced and obsoleted
Product Line:
Panelboards
Environment:
I-Line Panelboards
Resolution:
| I-Line Interior | Year | |
| Introduced | Obsoleted | |
| HCM | 1965 | 2020 |
| HCN | 1965 | 2017 |
| HCW | 1965 | 2005 |
| HCW-M | 1972 | 2005 |
| HCWA | 1978 | 1987 |
| HCP | 1979 | Current Offer |
| HCP-SU | 1979 | Current Offer |
| HCR-U | 1979 | Current Offer |
| HCWM-U | 1987 | 2004 |
| I-Line Combo | 2013 | Current Offer |
| HCJ | 2018 | Current Offer |
NOTE: The year introduced column is when they were first offered and the obsoleted column is when they were completely obsoleted.
Released for: Schneider Electric Canada