Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Does the NEMA 3R vented enclosures for NQ/NF panelboards uses the same lock as the non-vented NEMA 3R enclosures?

Product Line:

Panelboard NEMA 3R vented enclosures

Environment:

Low Voltage Panelboard

Cause:

Looking for similar enclosure that have the same lock that they can use for MH62D9VWP.

Resolution:

The new NEMA 3R vented enclosures uses a new lock with a unique key to that lock. It is different from the ones that we use on the standard NEMA 3R and NEMA 1 enclosures. Only way to get a replacement lock is to order it as special.

Schneider Electric Canada

Explore more
Product:
Users group

Discuss this topic with experts

Visit our community and get advice from experts and peers on this topic and more
Explore more
Product:
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
  • Register Your Product
  • Blog
  • Legal Information
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings