Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Is there a bus bar extension kit for 600A NQ interior like the NQ484L6C to put (18) 2-pole 125A breakers?

Issue:

Wants to put 18 pcs of a QOB2125 in NQ484L6C

Product Line:

NQ Panelboard

Environment:

Application

Resolution:

The maximum number of 125A 2P breakers that can be installed in a 600A NQ interior is 5 due to neutral port restrictions

It is a misapplication of an NQ lighting panel. It should be an I-LINE panel.

Schneider Electric Canada

Explore more
Product:
Users group

Discuss this topic with experts

Visit our community and get advice from experts and peers on this topic and more
Explore more
Product:
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
  • Register Your Product
  • Blog
  • Legal Information
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings