Issue:
To order standard deadfronts and filler plates replacements for series E1 NF panelboards.
Product Line:
Panelboard
Environment:
NF, Panelboard, Main Lugs Interior, Main Circuit Breaker Interior
Resolution:
For main lug interiors the entire deadfront is supplied as a replacement. Individual components are not available. Hardware is shipped with the deadfront. Deadfronts come without plastic filler plates. Filler plates are available as NFFP15.
For replacement of main circuit breaker interior deadfronts, only the main breaker section of the deadfront is listed below. To order an entire main circuit breaker interior deadfront, please order the appropriate Main Lug Interior deadfront from the table above, and a Main Circuit Breaker Interior deadfront from the table below.