Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Where is the physical connection or the location of the Coupling Capacitive Voltage Divider of the VPIS (Voltage Presence Indicating System) in the RM6 GIS switchgear?

Issue:

Customer wants to know the physical connection or the location of Coupling capacitive voltage divider with 30pF to 35pf in the RM6 GIS switchgear.

Product Line:

MV Gas Insulated Switchgear.

Environment:

RM6.

Resolution:

Please see below the image having marked capacitive voltage divider connection on the bushing in cable compartment. If VPIS is not in place in RM6 unit, then theses cables are connected to the earth.

image1

Schneider Electric Canada
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
  • Register Your Product
  • Blog
  • Legal Information
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings