Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
What is the Bus Bar Connection Hardware for PowerPacT M and P-Frame Circuit Breakers?

Issue: Identifying the catalog number of bus bar connection hardware for both M and P-frame MCCB

Product Line: PowerPacT M and P-Frame Molded Case Circuit Breakers

Resolution:

The bus bar connection hardware for one pole and one end of both M and P-frame breakers is S33928. It contains 1 quantity per kit.