Product Line:
Thermal Management Systems and ClimaSys
Environment:
ClimaSys CC Temperature Controller
Cause:
How to perform a Program Resetting or Factory Reset on the Electronic hygrotherm
Resolution:
Hygrotherm work in 3 different profiles, (M1 /M2 /M3) M1 by default programmed:
Operating Modes
- M1 Ventilation/Humidity and temperature control
- M2 Dew Point Control with alarm
- M3 Differencel Cools/Heats with the exterior temperature /Humidity and Temperature Control
To program reset this values it will be required to maintain both UP and DOWN button pressed at the same time, we will proceed to de-energize the controller without letting of the buttons and proceed to energize the unit, power the device once more, Resetting will erase the settings changed and the statistics (other than the total run time) and reset the device to factory settings.