Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
How to configure or adjust the response time on the ZBRRA receiver outputs

Product Line:
Industrial Wireless Remote Control.

Environment:
Receivers and wireless control stations.

Cause:
How to adjust the parameters on the wireless ZBR receivers outputs.

Resolution:

The outputs don´t have the possibility to modify the mono-stable time delay of this range, in fact it's duration is 500ms,  if you want to increase it's duration, a solution is to use an external timer and program this as per needed on the application.

Schneider Electric Canada

Explore more
Product:
Users group

Discuss this topic with experts

Visit our community and get advice from experts and peers on this topic and more
Explore more
Product:
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
  • Register Your Product
  • Blog
  • Legal Information
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings