Product Line:
Controllers for Industrial Machines
Environment:
Zelio Logic and Programmable Smart Relays
Cause:
How to change the programming language and module selection topology on Zelio Soft
Resolution:
Each program created on Zelio Soft is linked to a mapping or topology that needs to match our physical devices to be programmed, due to similar I/O needs for the program to detect, to change and verify this changes you may refer to the Module Tab.
After entering this menu we will see the programming language selection to either be Ladder or Function Block, we will select the ones that dictates our application:
Lastly to verify the module selection on the zelio soft, we will click the BACK button twice from this menu and we´ll be greeted with the module selection window, we will need to pick the correct commercial reference that according to the physical unit we´ll be programming to match the topology.