Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Can you add a Standalone Voltage Interface Module to the TeSys Island equipments?

Product Line:
Industrial Automation Control

Environment:
Motor Management Systems  TeSys Island

Cause:
Is it possible to add a standalone voltage interface module to the TeSys Island ?

Resolution:

The VIM is not a standalone avatar, therefore it cannot be used by it self , It is used in conjunction with another piece of equipment for voltage monitoring, such as a starter or load on our avatar topology.

If data monitoring is needed, you can suggest to use a PIM (Power Interface Module)

Schneider Electric Canada

Explore more
Product:
Range:
Users group

Discuss this topic with experts

Visit our community and get advice from experts and peers on this topic and more
Explore more
Product:
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
  • Register Your Product
  • Blog
  • Legal Information
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings