Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Zelio Programming: Can you transition an SR1 programming software to the SR2 cross on the Zelio Smart Relays?

Issue:

The program on a SR1 zelio soft 1 smart relay series can be transferred in the SR2/SR3 series of zelio soft 2?

Product Line:
Relays and Timers

Environment:
SR2 and SR3 Zelio Smart Relays


Resolution:

Yes, it is possible to convert the program from the SR1 to SR2. These are the steps:

Step 1 Download the program from the SR1 controller using Zelio Soft1 and save it. It will be saved as .zel format.

Step 2 In ZelioSoft2, select the Open existing program. From the dropdown in File type in open dialog box select *.zel format (Zelio Soft1 document) and select the file.

Step 3 Press open and it will automatically convert the application to Zelio Soft2 (.zm2).

You can reach us out at Tech Support area in order to check incompatibilities within software and product lines for Zelio Logic.

https://www.se.com/us/en/work/support/