Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
TeSys T Can you use or modify the current device topology on the current LTMR Device being used?

Product Line:
Industrial Automation Control

Environment:
Motor Management Systems TeSys T

Cause:
Can you use a program that was made for a specific device into another system topology? if so how to change this via SoMove?

Resolution:

We don´t suggest using different programs that are label for distinct commercial reference such as LTMR module or Expansion Modules being used, this will result on a error alarm that will ask us to re-verify the topology on our program.

There´s 2 ways that we can follow to change or Select the respective commercial reference being used on our current application:

By Creating a Bran New Program

Create Topology SoMove

Selecting the correct LTMR module and Expansion Modules that matches our physical commercial reference

Modifying the program topology on a actual created SoMove project

Edit Topology SoMove

Selecting the Device Tab on our SoMove Current project and clicking on Edit Topology

Edit Topology Window SoMove

This will open a new window that will allow us to modify the commercial reference for both Controller and Expansion module, it is mandatory to be connected to the current connected device in order to modify topology.

Schneider Electric Canada

Explore more
Range:
Users group

Discuss this topic with experts

Visit our community and get advice from experts and peers on this topic and more
Explore more
Range:
  • Products Documentation
  • Software Downloads
  • Product Selector
  • Product Substitution and Replacement
  • Help and Contact Center
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
  • Register Your Product
  • Blog
  • Legal Information
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings