Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
RE48 multifunction relay does not operate correctly after adjusting the time and function dials.

Issue:
RE48 multifunction relay does not operate correctly after adjusting the time and function dials.

Product Line:
Harmony RE48 panel mount timers


Environment:
Harmony multifunction relay


Cause:
After changing the function or time base of the multifunction relay the output doesn´t work as supposed to.


Resolution:
Modification of setting on potentiometers 4, 5, 6 is taken into account immediately. Modification of timing ranges or functions on switches 1, 2, 3, as well as the strap on terminals 2 and 6 L/Li should be carried out only with the power turned off. They will be taken into account at next switch-on or after Reset.

Schneider Electric Canada
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
  • Register Your Product
  • Blog
  • Legal Information
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings