Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
M580 and WRITE_PARM with EHC modules

Question: Can module parameters such as Modulo be programmatically changed when using high speed counter modules?

Answer: No, this is a limitation when the counter modules are mapped as Device DDT using Control Expert.

With the M580 incorporating Device DDT mapping, the adjustment parameters cannot be changed from the PLC application during operation (no support of READ_PARAM, WRITE_PARAM, SAVE_PARAM, RESTORE_PARAM) for:

  • counter modules in a Quantum EIO drop
  • counter modules in a M580 RIO drop

Schneider Electric Canada

Explore more
Product:
Users group

Discuss this topic with experts

Visit our community and get advice from experts and peers on this topic and more
Explore more
Product:
  • Products Documentation
  • Software Downloads
  • Product Selector
  • Product Substitution and Replacement
  • Help and Contact Center
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
  • Register Your Product
  • Blog
  • Legal Information
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings