Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
What is the replacement mounting screw for installing an L-frame breaker inside I-Line panelboard?

Article available in these languages: Spanish

Issue:

What is the replacement part # of a mounting screw for a Powerpact L frame breaker I-line mounting bracket?

Product Line:
PowerPacT L-frame

Resolution:

There is no commercial part number available for this screw, and it is not sold separately. However, a 10-32 x 5/8 screw can be used for mounting a PowerPact L-frame breaker inside an I-Line panelboard.