Issue
Phasor angles are not available in IEC 61850 M03_MMXU1 Module for the ION8650 meter. How can I map the Phase Angles in my IEC 61850 CID file.
Product Line
ION8650
Environment
IEC61850 CID Files
Cause
Cannot view Phase Angle data points for LD0.M03_MMXU1.A.phsA.cval.ang.f
Resolution
- For the ION8650 meters, the phase angle data is not in the MMXU module. The data can be found in the IEC 61850 MHAI module for Phase voltage, line to line voltage, and currents.
- If reading the MHAI module does not work for the customer, the other option would be to link the phase angles to the custom analog node.
- For more information on ION modules, please refer to the ION Reference.