Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
What are the new features of EcoStruxure Control Expert V16.2?

Issue:

New features of EcoStruxure Control Expert V16.2


Product Line:

EcoStruxure Control Expert


Resolution:

The new features of Control Expert V16.2 are listed below

• TÜV Certification achieved for EcoStruxure Control Expert V16.2.

• Enhanced support of Modicon M580 controller firmware V4.40.

• Modicon Edge I/O NTS support implemented in EcoStruxure Control Expert Classic.

• Comprehensive support of Modicon M580 BMENOC0302(H) module.

• Bandwidth limit calculation adjustment for the controller and the Modicon M580 BMENOC0302(H) communication module over backplane with Serial Network Access Protocol (SNAP).

• Manageable download script creation for IKEv2 for Modicon M580 BMENOC0302(H) module in EcoStruxure Control Expert Classic and EcoStruxure Control Expert (Topology Manager).

• Programming environment. Customizable FBD comment color selection options.

• Uninstalling EcoStruxure Control Expert 16.2 removes the DTMs that were installed with this version. The installation packages of these DTM Libraries are provided in the DTM_Installers folder of the EcoStruxure Control Expert installation package (.iso). You can use them to individually remove or reinstall DTMs