Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Is there an EIFE module available for fixed-type version of MTZ breakers?

Article available in these languages: Spanish

Issue:

Installing the EIFE on fixed MTZ breaker version

Product Line:

Masterpact MTZ1, MTZ2, MTZ3

Resolution:

No, the EIFE (Embedded Ethernet Interface) module is not available for fixed-type Masterpact MTZ breakers. It is designed exclusively for drawout-type MTZ1, MTZ2, and MTZ3 breakers.

The EIFE module requires the ULP port for drawout breakers that goes mounted on the cradle. Therefore, it cannot be mounted or connected to fixed-type breakers. If you're working with fixed MTZ breakers and need Ethernet connectivity or remote monitoring, you can use an IFE module.

Related Part Numbers:

LV851200SP – Replacement EIFE kit for drawout-type breakers

LV851001SP – Standalone EIFE module replacement for drawout breakers

LV434001 - IFE Ethernet interface for one breaker

LV434002 - IFE Ethernet interface gateway

Schneider Electric Canada
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
  • Register Your Product
  • Blog
  • Legal Information
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings