Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
What is the highest breaker allow in a HCJ and HCP I-line Panelboards?

Subject:

Maximum Breaker Ratings for HCJ and HCP I-Line Panelboards
Language:

English
Issue:

Determining the highest allowable breaker sizes for HCJ and HCP panelboards
Product Line:

Schneider Electric I-Line Panelboards
Resolution:

  • HCJ Panelboard:

    • Maximum branch circuit breaker rating: 250A
    • Compatible breaker types: BD, BG, BJ, QB, QD, QG, QJ, HD, HG, HJ, HL, HR, JD, JG, JJ, JL, JR
  • HCP-SU Panelboard:

    • Maximum main circuit breaker rating: 800A
    • Maximum branch circuit breaker rating: 600A
    • Compatible breaker types:
      BD, BG, BJ, LA, LG, LJ, LL, LH, LR, MG, MJ, PG, PJ, PL, PGC, PJC, PLC, QB, QD, QG, QJ, HD, HG, HJ, HL, JD, JG, JJ, JL

Note: PG, PJ, and PL breakers are available in both thermal-magnetic and MicroLogic trip versions. MicroLogic breakers are offered in 80% and 100% rated configurations. A “C” suffix indicates a 100% rating.

For specific configurations such as HCP54868SU, refer to catalog numbers like HC2686T()4P, HC2686DB, and HC2886WP for detailed

Schneider Electric Canada
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
  • Register Your Product
  • Blog
  • Legal Information
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings