Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
What is the weight of the HCP32686 Interior Panelbaord?

Article available in these languages: Spanish

Issue:
Finding the package weight for the HCP32686 panelboard

Product Line:
Schneider Electric Panelboards

Resolution:
The HCP32686 panelboard has the following packaging weight:

  • Package Weight (kg): 72.575 kg
  • Package Weight (lbs): 160.0006 lb (US)

This information is useful when planning for shipping, handling, or installation logistics.

Schneider Electric Canada

Attachment(s)
Square_D_HCP32686_Specification_Sheet.pdf [261.75 KB]