Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
What is the switching life and mechanical life of a vacuum contactor?

Article available in these languages: Spanish

Issue:
What is the switching life and mechanical life of a vacuum contactor?

Product Line:
Motorpact™ 200/400/450 A Vacuum Contactors

Environment:
Replacement and maintenance planning

Cause:
Determining when it is necessary to replace the vacuum interrupter based on operational limits.

Resolution:

  • Switching Life: The vacuum interrupter should be replaced after reaching its switching life of 250,000 operations.
  • Mechanical Life: The overall mechanical life of the contactor is rated at 2,500,000 operations.

Source:
Motorpact™ 200/400/450 A Vacuum Contactors – Instruction Bulletin 46032-700-02D (03/2011)

Schneider Electric Canada

Attachment(s)
46032-700-02D (1).pdf [1.34 MB]
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
  • Register Your Product
  • Blog
  • Legal Information
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings