Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
What is an EcoStruxure Site Server?

Issue

This a new device “EcoStruxure Site Server” and needs to be revealed to user

Product Line

EcoStruxure Site Server/ Harmony P6

Environment

Documentation

Configuration

Cause

The device seems to be unknown and needs detail information.

Resolution

When searching for documentation on the Site Server—whether on SE.com or through Google—it’s best to use the term “EcoStruxure Site Server”.

The EcoStruxure Site Server (ESS) is an Internet of Things (IoT) gateway designed to enable cloud-based energy management services as part of the EcoStruxure architecture. It provides a secure connection to the Schneider Electric (SE) cloud, allowing you to safely access information, optimize your power system, and achieve sustainability goals for energy efficiency.

EcoStruxure Site Server is an accessory for EcoStruxure Energy Hub (EEH). It is manufactured under the Harmony P6 product line but configured as a gateway for the EEH system.

Fig. 1: EcoStruxure Site Server

Site Server device

It is powerful IoT gateway with enhanced cybersecurity, Site Server connects the entire site’s electrical and energy network. Onboard web pages allow you to connect and configure power and energy meters, intelligent circuit breakers and other metered electrical assets and push this data to the cloud.

It can be order like any other PowerLogic/ ION product, and has mostly (4) parts numbers:

  1. PSWSSUD1A: for Universal DC power control and communicates over Ethernet
  2. PSWSSUA1A: for Universal AC power control and communicates over Ethernet
  3. PSWSSUD2A: for Universal DC power control and communicates over Ethernet and RS-485
  4. PSWSSUA2A: for Universal AC power control and communicates over Ethernet and RS-485.

The EcoStruxure Site Server is a Windows-based PC device, similar to a computer, that includes a version of Power Monitoring Expert (PME) software. It comes with a license activation ID for PME and a device key that enables secure cloud connectivity. This information is provided on a label located on the back of the unit.

Also, the Site Server can be offered as a standalone device or housed in an enclosure, model FAEMGW1PDXN (see attachment).

Fig. 2: EcoStruxure Site Server label

Site Server label

  1. WinUser: Site Server username for windows user access
  2. WinPwd: Site Server password for windows user access
  3. WebUser: Site Server username for webpage user access
  4. WebPwd: Site Server password for webpage user access
  5. ServerName: Site Server name for cloud access
  6. SiteKey: Site Server key to set it for identification in the cloud
  7. ActID: Site Server activation ID or license activation ID

For security reasons, the font size of the characters is reduced, allowing the QR code to be scanned to access and download the label information.

Documentation

Schneider Electric Canada

Attachment(s)
FAEMGW1PDXN.pdf [524.28 KB]
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
  • Register Your Product
  • Blog
  • Legal Information
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings