Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Operator Terminal Expert ModbusSIO driver, can not import Control Expert XVM file.

Issue:

In EcoStruxure operator Terminal Expert, using the ModbusSIO (serial) driver, it cannot import the variables from a Control Expert .XVM file.

Product Line:

EcoStruxure Operator Terminal Expert (all versions).

Resolution:

For now, EOTE doesn't support importing the Symbol Link from the XVM file using the Modbus serial driver (ModbusSIO).

The recommended solution would be to use the ModbusTCPIP driver and communicate via Ethernet.

If this is not possible, then the variables need to be created manually in the EOTE project.

With the ModbusTCPIP driver are not only the located address variables, but also the unlocated address variables are supported.

There is no plan to support this feature with the ModbusSIO driver in a future release of EOTE.

If this FAQ did not solve your issue, you can chat with us at chat with us or e-mail us at customer.services@se.com to create a case with our Technical Support Team.

If you are not located in North America, please contact your local Customer Care Center for assistance: Support | Schneider Electric Global (se.com)