Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
How to replace SR2MOD02 / 03

Title: How to replace SR2MOD

Issue: SR2MOD is now obsolete

Product Line: SR2 Smart Relays

Environment: SR2MOD Communication

Resolution:

SR2MOD02/SR2MOD03 modems are no longer commercialized.

In order to propose an alternative to our customers, we tested the TRB142 modem from Teltonika with our controllers.

Moreover, this modem is 4G compatible by comparison with SR2MOD02/SR2MOD03.

Regarding the customer's need, in order to get an SMS from the Zelio, you need to have:

- Zelio Module (ref: SR2B, SR2E or SR3B only)

- SR2COM01 with FW >= V1.0.14 (see FAQ)

- SR2CBL07 cable with the marking H2.0 (otherwise the cable cannot be used with TRB142 modem)

- TRB142 modem

Currently, the SR2CBL07 H2.0 cable is not available as accessory, it is included when ordering the SR2COM01.

Info from the Datasheet:

=> SR2A101BD module is not compatible with SR2COM01.

Link to the Quick Start Guide :

https://download.schneider-electric.com/files?p_enDocType=Instruction+sheet&p_File_Name=1602234_01_11_A05.pdf&p_Doc_Ref=1602234_01A55

As mentionned in the FAQ, it could be needed to update the FW of the SR2COM01 and use ZelioSoft V5.4.2.

Schneider Electric Canada

Explore more
Product:
Users group

Discuss this topic with experts

Visit our community and get advice from experts and peers on this topic and more
Explore more
Product:
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
  • Register Your Product
  • Blog
  • Legal Information
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings