Vores varemærker

Velkommen til Schneider Electrics website

Velkommen til vores website
		
Hvordan kan vi hjælpe dig i dag?
What are the minimum clearances for mounting an ATS48?

Issue:
Minimum clearances required on the ATS48 soft starters?

Product line:
Altistart 48, ATS48

Environment:
all

Cause:
Mounting inside an enclosure

Resolution:
There is a minimum of 4 inches (100 mm) on the top and bottom of the softstart. A minimum clearance of 2 inches (50mm) on each sides.
The enclosure must also allow for proper ventilation to maintain a maximum temperature of 40C (104F) and provide required wire bending space.

If this FAQ did not solve your issue, you can call us at 1-888-778-2733 Option 2 and then 4 or e-mail us at drive.products.support@se.com to create a case with our Technical Support Team.