Hvordan kan vi hjælpe dig i dag?

What is the maximum operating altitude for Altivar 71 Drives.

Altivar 71 Drives are designed to operate for altitude up to 3000 Meters.

Note:

The maximum operating altitude is 1000 Meters, after which you have to derate the Altivar 71 Drive 1% per additional 100 Mtrs. over 1000 Mtrs. up to 3000 Mtrs.