Is it possible to order a 300 amp MCC feeder bucket for Model 5 or 6?
Issue:
Order a 300 amp MCC feeder bucket for Model 5 or 6
Product Line:
Motor Control Centers.
Environment:
Products sold in the United States.
Cause:
Product features.
Resolution:
Yes. A 300A circuit breaker feeder bucket is available in a 24`` branch unit. There is also the posibility to have a 300A feeder bucket with the "High Density Branch Feeder Selection" in a 6" bucket. Note this would have to be worked up on the SE Advantage Product Selector.