What is the part number for the cooling fan for the ATV71HD15N4?
Issue:
Is there a spare parts part number for the heatsink fan kit for the ATV61HD15N4 or ATV71HD15N4
Product Line:
Altivar 61 and Altivar 71
Environment:
AC Drives and Softstarts
Cause:
Heatsink Fan Spare or Replacement parts
Resolution:
VZ3V1205 is the heatsink fan kit. The fan measures 3.14 by 1.5 inches.
Ordering Qty is 1 fan kit per drive.
The Kit Includes 2 Fans and the mounting adapter plate.
CTA-ID : 2061517
Udgivet til: Schneider Electric Danmark