Does Schneider offer a drive that has connections to the DC bus for putting the regenerative voltage back onto the utility line?
Issue:
Drive offer with connections to the DC bus for putting the regenerative voltage back onto the utility line
Product Line:
Altivar Process 980
Environment:
NA
Cause:
Regenerative voltage back on the utility line
Resolution:
The Process 980 product line is an Active Front End (AFE) drive for regenerative applications.