Hvordan kan vi hjælpe dig i dag?

Video: Increasing ATV21 & ATV212 High Speed Setting Beyond 60Hz.

Issue:
ATV212 and ATV12 High Speed Setting Beyond 60Hz.

Product Line:
ATV21 ATV212 S-Flex

Environment:
All serial numbers

Cause:
Overspeed operation is desired.

Resolution:
First, set the maximum frequency, FH, to at least the desired high speed.
Second, change the upper limit, UL, to the desired high speed.

If an analog input is used for speed reference, it will need to be scaled:
If FMOd=1, VIA analog input, then set F204 to the high speed.
If FMOd=2, VIB analog input, then set F213 to the high speed.