Hvordan kan vi hjælpe dig i dag?

Can a VW3A1101 keypad be used on the ATV312 to transfer programs?

Issue:
Store and transfer program files using VW3A1101 keypad.

Product Line:
Altivar ATV312

Environment:
All models, all serial numbers.

Cause:
A duplicate program is to be used on multiple drives.

Resolution:
No.  Although the VW3A1101 is compatible with ATV312, it cannot be used to transfer a program file from one ATV312 to another.  A Multi-Loader or Simple Loader tool or SoMove software can be used to transfer files.

If this FAQ did not solve your issue, you can call us at 1-888-778-2733 Option 2 and then 4 or e-mail us at drive.products.support@se.com to create a case with our Technical Support Team.