Hvordan kan vi hjælpe dig i dag?

How do you wire up a 2-wire or 3-wire transducer to the S-Flex 212 Drive?

Issue:
Wiring up a 2-wire or 3-wire transducer to the S-Flex 212 Drive.

Product Line:
S-Flex 212 and 21

Environment:
All

Cause:
Needs to wire in a 3 wire 4-20mA transducer to the S-Flex 212 drive.

Resolution:
3 wire transducer:
P24
VIA  (4-20mA)
CC

2 wire transducer:
P24
VIA (4-20mA)