What is the serial cable to connect an XBTN200, XBTN400 and XBTR400 HMI to a Modicon M340?
The XBTZ9980 cable allow the communication between Modicon M340 PLC series through Modbus RJ45 port and the following HMI PRODUCTS: XBTN200, XBTN400 and XBTR400.
-Specifications:
-Connectors
XBT side J1 : RJ45 Male 8 points
PLC side J2 : RJ45 Male 8 points
-Length
2.5m
-Temperature
Working temperature : -20°C to +70°C
Storage temperature : -40°C to +80°C
-Certification
CE certified and CSA UL508
Fireproofing rating : UL VW-1 for the cable
ROHS compliance