How can I read a string data from OFS V3.60?
1) The typical syntax AliasName!%MW returns the numerical value of the string.
2) To see the actual data in a string format you need to add the ;c at the end.
AliasName!%MemoryWord;c
M340!%MW10:4;c
Udgivet til: Schneider Electric Danmark