Hvordan kan vi hjælpe dig i dag?

How to get access on ILX2T?

Goals and Symptoms

How to get access on ILX2T?

Causes and Fixes

To write parameters via Modbus TCP, e.g. the control word, the plc must take the access rights before. This happens by writing the value 1 to parameter 282.

Attention:
This is not necessary if the IOscanning with Unit-ID 255 is used.


Legacy KB System (APS) Data: RESL201667 V1.0, Originally authored by PaFr on 03/18/2010, Last Edited by PaFr on 03/18/2010
Related ranges: Lexium ILA, ILE, ILS