Hvordan kan vi hjælpe dig i dag?

Why do I get the error code OL9-21581 Illegal Modbus function code when trying to connect to the Concept simulator?


One possible reason is the package of Concept installed is Concept S or Concept Small. The small version of Concept does not contain the IEC 32 simulator.