Hvordan kan vi hjælpe dig i dag?

Can I move documentation information from one 884 database to another 884 database using the ProWorx 884 software?

Issue

Can I move documentation information from one 884 database to another 884 database using ProWorx 884 software?

Product Line

ProWorx

Environment

ProWorx 884

Resolution

Yes you can move ProWorx 884 documentation from one 884 database to another 884 database. You would first need to export the documentation from the existing 884 database by creating a *.FIL file. You can then import this *.FIL file into the other 884 database.