Hvordan kan vi hjælpe dig i dag?

Impossible to run PL7, Concept and XBTEL setup. No error message displayed

Goals and Symptoms

Impossible to run PL7, Concept and XBTEL setup.
No error message displayed

Causes and Fixes

Cause: Sunbelt Kerio Personal Firewall installed

Fixes: - Uninstall Kerio or
- In the task bar, right click on the Kerio icon and select Quit (each time an installation is required)


Legacy KB System (APS) Data: RESL179815 V1.0, Originally authored by on , Last Edited by LaBa on 09/22/2006
Related ranges: PL7