Hvordan kan vi hjælpe dig i dag?

What are the features of the BMXRWSFC032M memory card for the BMXNOE0110?

The BMXRWSFC032M is a 32MB memory and when inserted in the FactoryCast option module BMXNOE0110, it provides services to conform to Transparent Ready class C30. A total of 32MB are available for user web pages and the BMXNOE0110 is delivered with one BMXRWSFC032M already installed.