Does the M340 CPU support e-mail with Unity Pro 4.0?
Issue:
Clarification is needed on whether M340 CPUs support e‑mail functionality when using Unity Pro 4.0.
Product Line:
Modicon M340
Unity Pro 4.0
Environment:
Unity Pro 4.0
M340 CPU with embedded Ethernet
Resolution:
Yes. E‑mail is supported, with the following limitations:
Outgoing e‑mail only (no incoming e‑mail support).
Supported only on M340 CPU modules with embedded Ethernet ports.
Examples of supported CPUs:
BMXP342020
BMXP342030
CPUs without embedded Ethernet do not support e‑mail functionality in Unity Pro 4.0