Hvordan kan vi hjælpe dig i dag?

When ordering a Quantum I/O modules does the field wiring connector come with it ?

No, the 40-pin field wiring connector has to be ordered separately for all the I/O modules. The part number is 140XTS00200.


Note: The Quantum line will be obsoleted 12/31/18 and should be replaced with the M580 and x80 I/O.



R-82117