Which IODDT data type would I use for an M340 analog input module that includes the input value and other channel information?
Issue:
Which IODDT data type would I use for an M340 analog input module that includes the input value and other channel information?
Product Line:
M340 analog input module
Resolution:
The IODDT for all channel properties is T_ANA_IN_BMX..
This Data Type will yield all of the channel's properties and diagnostic information.
If you only want the channel VALUE and CH_ERROR properties you can use the T_ANA_IN_GEN Data Type.
If this FAQ did not solve your issue, you can chat with us at chat with us or e-mail us at customer.services@se.com to create a case with our Technical Support Team.
If you are not located in North America, please contact your local Customer Care Center for assistance: