Instructions on how to set the time on an ION73xx meter using modbus
Issue
Instructions on how to set the time on an ION73xx meter using Modbus.
Product Line
ION7300 Series (ION7300, ION7330, ION7350)
Environment
ION73xx meters – Time configuration using Modbus protocol
Resolution
Using the Modbus protocol, it is possible to set the time on ION7300 series meters. This process is not a time synchronization (since there is no external source continuously sending a signal), but you can use Modbus software to automate the process by retrieving time from a source and passing it to the meter.
To set the Meter time via Modbus communications do the following:
1. Set the ION Clock Module Time Sync Source Register to the Modbus
communications port.
2. Write the UNIX time in seconds as an unsigned 32-bit value to Modbus
Registers 41926 (high order) and 41927 (low order).
Steps to Set Time via Modbus
- Convert the desired time to UNIX time (seconds since 01/01/1970 UTC).
- Split the UNIX time into two 16-bit values:
- Lower order 16 bits → Register 41927
- Higher order 16 bits → Register 41926
Example
- UTC Time: 07/01/2009 02:00:01 AM
- UNIX Time: 1246413600 (decimal)
- Binary: 0100 1010 0100 1010 1100 0011 0010 0000
- Lower order bits: 1100 0011 0010 0000 → 49952 (decimal)
- Higher order bits: 0100 1010 0100 1010 → 19018 (decimal)
Write:
- 49952 to register 41927
- 19018 to register 41926
The meter will now display the correct time and continue ticking based on its internal clock.