What is the Dielectric Withstand Voltage of the ION6200 Communications Port?
Issue
What is the Dielectric Withstand Voltage of the ION6200 Communications Port?
Product Line
ION6200 Power Meter
Environment
ION6200 RS-485 Communications Port
Resolution
The maximum voltage that can be applied to the RS-485 communications port in the ION6200 is 7.5 Volts.
Udgivet til: Schneider Electric Danmark