Hvordan kan vi hjælpe dig i dag?

Is there a way to stop a ION6200 meter's display from scrolling?

Product Line
ION6200

Resolution
There is a setting which is configurable from the front display setup which affects the scroll rate of the display.
dScr
Display Scroll Time

By default this is set to 0, but can be increased from 1 second to 30 seconds.