Hvordan kan vi hjælpe dig i dag?

May the Energy Meter Communications Board be added to the Energy Meter in the field?

Issue
Can the Energy Meter Communications Board be added to the Energy Meter in the field?

Product Line
Energy Meter
Energy Meter Communication Board

Environment
Communications
Field Retrofit

Resolution
Yes, the Energy Meter Communication Board (EMCB) may be installed in the Energy Meter in the field.
See chapter 3 of the Energy Meter Communication Board Instruction Bulletin attached below.

Schneider Electric Danmark

Bilag
Energy_Meter_Communication_Board.pdf [913.79 KB]