How to configure the Momentum to start in RUN mode after a power cycle using Modsoft
Issue
How to configure a Momentum start in 'RUN' mode after a power cycle using Modsoft.
Product Line
All Momentum PLC's.
Environment
Windows 7
Resolution
In order for the Momentum to start in RUN mode after power cycle, the program must be saved to the built-in flash.
The following steps can be used to accomplish this in 'Modsoft version 2.62.
- Click Online\ Direct To PLC.
- Press F2 'PlcOps'.
- Press F2 to 'Stop the PLC'.
- Press F8 'Save To'.
- Type in Y for answering the question (Continue Power Down Run State?).
- Type in Y for 'Continue'.
- Press F1 to 'Start the PLC'.
- Disconnect from the PLC.
- Power cycle the PLC and it will start back up in RUN mode.