What is the maximum pulse output rate of PM700P ?
Issue
What is the maximum pulse output rate of the PM700P meter?
Product Line
PowerLogic™ PM700P Series Meter.
Environment
Applications requiring pulse output for energy monitoring, data logging, or integration with external systems such as building management systems (BMS) or SCADA.
Resolution
The pulse output of the PM700P meter can operate at a frequency of up to 9.8 Hz.