Where can one find max line current values for the ATV312 drives?
Issue:
Max line current values for the ATV312.
Product Line:
Altivar ATV312
Environment:
All
Cause:
Input line currents for the ATV312 drives.
Resolution:
The input line supply values are going to be for voltages between 200VAC to 240VAC or 380VAC to 500VAC 50/60hz.
See the ATV312 install manual document bbv46391 page 10 thru 11 for line current max values.
https://www.schneider-electric.com/en/download/document/BBV46391/
Udgivet til: Schneider Electric Danmark